AXIS#.MOTOR.TBRAKEAPP

Description

This parameter is the mechanical delay required for the motor brake to close. When disabling an axis using AXIS#.DISMODE not '0 - Disable axis immediately', the drive will servo to hold position for this time delay, allowing the brake to apply.


  • AXIS#.MOTOR.TBRAKEAPP has no effect when DISMODE is 0.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 1,000 ms

Default Value

75 ms

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.TBRAKEAPP

500bh

1ah

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.TBRAKEAPP

510bh

1ah

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6215

1

6215 (0x1847)

AXIS1.MOTOR.TBRAKEAPP

Unsigned16

Read Only

Yes

71751

2

6215 (0x1847)

AXIS2.MOTOR.TBRAKEAPP

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TBRAKEAPP

6215

Unsigned16

Read Only

-